Other Parts Discussed in Thread: INA219
Hello,
working on a project where up to 25A AC current is used and must be measured. We decided to go with Honywell S&C CSNX25 (http://sensing.honeywell.com/index.php?ci_id=3108&la_id=1&pr_id=4967) closed loop current sensor. Output current should be between 12mA and 12,5mA and I would like to measure this with standard ADC with 3,3V reference. Since this is 0V/5V powered device it has it's own reference voltage at 2,5V. From this current measurement resistor was found to be 200R.
Now, I need to detect this AC current and transfer it to 0V to 3,3V output.
Is anyone who had same situation? Anyone saw any application note or there is already TI's solution for my problem? :-)
Thank you for help,
Andrej