Other Parts Discussed in Thread: LM111
Hi,
I want to use the LM111 Voltage Comparator but in order to do so, I need you to clarify the following points (Attached Simulation):
1. Simulation is not pin compatible to the component datasheet (simulation missing pin 6: BALANCE/STROBE and pin 5: BALANCE).
2. How can I create hysteresis of ~2.5V and ~1V (I have 0V-5V square wave input)? Is it possible to do so if my load will be ~1k ohm? (My attention is to connect the LM111 output pin to cathode of the High Speed opto-coupler. The anode will be connected to 12V through 1kohm serial resistor)
3. Why 10V zener diode, become active at 6V? (Change the amplitude to 10V with DC of 10V)
4. Do you see any reason to split the R1 resistor into two resistors: before and after the zener (adding addition resistor next to the LM111 + pin)?
Idan