Other Parts Discussed in Thread: THS7360, OPA3695
Dear all,
Recently, I encounter a signal quality issue about Analog RGB signal.
I measure the VESA spec. The spec of rise/fall time is 1.66ns if resolution is 1080P 60Hz.
If you want to achieve the 1.66ns of rise/fall time, it means the bandwidth of THS7360 must be large than 210MHz (0.35/Tr)
But, DM8168EVM set the filter of THS7360 to 70MHz as below.
So, it cause the rise/fall time on our board is impossible to meet the spec.
The table shown below is my test result.
Can anyone help to explain this setting is reasonable and the DM8168EVM have any test result on VGA signal for VESA spec? Thanks in advance.
B.R.
OC