Other Parts Discussed in Thread: XTR111
Hello,
I am using an XTR111 with the attached schematics; the IC is powered at 24 V, and the input is at 5 V (more precisely, it is 5.1 V). The problem is XTR111 output saturates at 19.4 mA, and I'm not able to understand why. I have four identical circuits, and all of them share the same problem, so I think there must be something wrong in my schematics. JP1 is used for selecting voltage or current output, and is removed at the moment.
Can you please help?
Thanks in advance,
Stefano