Other Parts Discussed in Thread: TLV2373, TLV2372
I am using TLV2373 as an amplifier in single supply mode. since the input signal to the amplifier contains both dc and ac voltages. so in order to decouple dc from the amplified signal i am using a decoupling capacitor at the output but after decoupling i am not getting a symmetrical ac output. why it is so.
i am also uploading the schematic of the circuit as well as the input and output waveform. The 2nd image is of applied input signal & the 3rd image is amplified voltage at the output if the TLV2372 & 4th image is of the voltage signal after dc decoupling.
regards
Akhilesh Sati