Other Parts Discussed in Thread: INA121, INA111
I'm interested in using the INA121 in a capacitive bridge transducer circuit but there is absolutely nothing written about the circuit except the circuit diagram in FIGURE 11. I'm using 40KHz for Vac with matching 100K ohm resistors with the values of the capacitors around 0.8pF. I'm also power the in-amp with +/-5V. Problem is with the output of the transducers and the gain that I'd like to use. Are there app notes or something that I could refer to with this circuit. I've worked with in-amps before and I'm aware of the problems but this circuit just doesn't give me the gain I would expect.
Thanks, Mark