Other Parts Discussed in Thread: OPA847, LMH6629, OPA684, BUF602, OPA4820
In my application, I have a voltage signal that is like a radar pulse.
It is at a 5MHz sine wave, lasts a few microseconds, and is (as far as I can tell) about 1uV in amplitude. I need to amplify it to 1.0 volt or so.
I can not determine the source impedance but I think it is quite low.
I have tried a few variations of amplifers and can get the signal high enough but the noise is killing me. So I thought I would use a low noise first stage with a gain of 10 then maybe three more stages with voltage gains of V/V=20 (21.5 to be exact). I thought that if each of the three stages had 2 pole BP filters on them I might get the noise low enough. Any supply voltage other than 5.0 would be a problem I hope to avoid.
Please comment on my plans. Also suggest a circuit and components if possible.
Thanks In Advance,
Pete