Hi, I was just wondering if there is any coupling between the two input/output sets in dual opamps, such as the OPA 2604.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, I was just wondering if there is any coupling between the two input/output sets in dual opamps, such as the OPA 2604.
Aaron,
There will always be some degree of crosstalk between channels on dual (or triple, quad, etc) op amp packages. Whether it's significant or not is the question; many amplifiers specify "Crosstalk" as the metric for seperation. This particular part specifies crosstalk as "channel seperation." The datasheet shows 142dB at f=1kHz and Rl=1k Ohm. There's also a chart on page 6 labeled "Channel Seperation vs. Frequency" that shows the crosstalk performance over a wider frequency range.