Other Parts Discussed in Thread: OPA835, OPA836, OPA2889, THS4281, OPA890, LMH6618, LMH6645, OPA683, LMH6723, OPA684
do you have suggestion part to replace LT6233-10?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Jeff,
TI does not have an exact replacement to the LT6233-10 (decompensated version). But, depending on what your circuit needs are, we may have some options to consider. I will throw several options to consider below. But, if you can share what your specific key care-abouts are, then I may be able to narrow things down quickly. I will assume low power is a key concern so I will start with that. Keep in mind that Voltage Feedback (VFB) amplifiers do have a gain-bandwidth (GBW) product rule so as gain increases, bandwidth is reduced.
a) OPA835 : RRO, up to 5V single supply, Iq = 250uA, 56MHz
b) OPA836: RRO, up to 5V single supply, Iq = 1mA, 205MHz
c) OPA2889, Dual, up to 12V single supply, Iq = 460uA/ch, 60MHz @ G=2
d) THS4281, RRIO, up to 15V single supply, Iq = 750uA, 90MHz
e) OPA890, up to 12V single supply, Iq = 1.1mA, 115MHz @ G=2
f) LMH6618, RRIO, up to 11V single supply, Iq = 1.25mA, 130MHz
g) LMH6645, RRIO, up to 12V single supply, Iq = 650uA, 55MHz
Another opiton to consider is to go to a Current Feedback Amplifier for high gain. this is because CFB amps do not have a GBW product limitation as much as VFB amps do. There are pros and cons of a CFB vs VFB, but in many cases a CFB will work without issues.
h) OPA683, up to 12V single supply, Iq = 940uA, 94MHz @ G=10
i) LMH6723, up to 12V single supply, Iq = 1mA, 200MHz @ G = 6
j) OPA684, up to 12V single supply, Iq = 1.7mA, 120MHz @ G = 10
Cheers,
Randy