Hi there, i'm using a XTR117 to study the voltage-to-current method for 4-20mA output signal, this is the only ic available for me at this moment (ordered a xtr101, seems to be more flexible, i`m right?).
i print a pcb to solder the xtr and i've tested it following the diagram on pg1 of datasheet using a potentiometer as sensor:
Where:
R1 = 10k Ohm
R3 = 8k Ohm
R2 = 250 Ohm
Vcc = 9 v
i'm using a multimeter to measure the voltage on the R2 (the load) and the variation on the voltage it's 10mV maximum...if i plug the multimeter to measure current in serial with the load got 20mA of measuring and no variation.
after burn my brain and make a lot of testings, including using a dataTaker DT82E (amazing machine!) to measure current loop ...nothing happens..
so.. i unplug my "sensor" and just feed the xtr with vcc, if i measure Vreg with Iret, i've got only 3.59v! must be 5v, right?
i'm totally lost, can anyone help me?