Other Parts Discussed in Thread: OPA335
I want to use the current from the load to ground to control a pulse. I have used a resistor to start with. To get a suitable reaction I used a 0,33Ohm' resistor for 1,75 Amps,it gave the required control voltage of 0,58V. The loses of 058V x 1,75 Amps is not what I want so I want to jump to an op.amp...
Is the opa335 a moderade ,suitable advice to achieve the benefit of less in losses, a package of TSOT-23 and not less in pitch. The reaction I don't really know ,but say a reaction `nearly` as quick reaction dynamically as the resistor at changes in loads. We talk of load steps of say I amp.
Please advice me if you see the opa 335 as a not a too bad suggestion or something else not more complicated but far better. Please give me a circuit drawing that will fit as well..