Other Parts Discussed in Thread: INA214
Hi,
I have a problem with the INA214. I use a 5mR shunt resistor in my current measurement. At 1A I get 150mV at the output of the INA214, at 2A 300mV, but it is supposed to have a gain of 100V/V. Supply voltage is 3.3V and the REF input is tied to ground.
I double checked the case marking, it is indeed an INA214. Do I miss something?
Thanks for the help