Other Parts Discussed in Thread: INA122, XTR106
Hi,
I am in the process of designing a scale with max weight set at 10KG (22.046LBS) I am using the INA122 as my instrumentation amplifier. I am using a Wheatstone bridge circuit to detect the difference in my voltages with the weight differences. I am using two strain gauges both 350 ohm and two 350 ohm precision resistors. My voltage source is 5V. The problem I am having is I am not getting any output on the amplifier. When the bridge is balanced 0v = Vout = 0KG. Max weight should equal about 10 mV(ish) difference VA and VB and then I set the gain equal to 500 on the amplifier to set it to 5v = my max weight of the scale. Still no output on the amplifier. If I have it balanced I get the 0KG. If I don't have one leg of the bridge hooked up to the amplifier I get 5v out on Vout = 10KG. I am having problems with the in between portion of the amplifier. I am attached a picture of my schematic. Vout of the INA122 going is to the ADC of a P18F4550 microcontroller.
Thanks for your help
Bryden Smith