Other Parts Discussed in Thread: LM2901, LM2903, LM2903-Q1, LM2901-Q1
Hello,
I am using LM2903/LM2901 as comparator with hysteresis to interface a variable reluctance (VR) sensor (Frequency measurement) with microcontroller.
Please find below a few queries on LM2903/LM2901:
a) What is the recommended value of capacitor (min to max) between the inverting and non- inverting inputs of comparator to avoid oscillations?
b) What is the maximum current a I/P pin could withstand? The input voltage range is listed as −0.3 V to 36 V but what is the max. current carrying capability of pin?
FYI: My application has a VR sensor that outputs a sine wave pulse of maximum amplitude 120Vp-p with max. frequency 10KHz depending upon the target speed.
c) Could bias current specifications be considered as leakage current?
Thanks and Best Regards,
Swati