Other Parts Discussed in Thread: INA230
Hi, I am interested in design a system to measure DC power. The voltage to measure is between 2.7 to 4.2 Vots and the current between 1uA to 200mA.
Could I use the INA230 IC?
What resistance value must I use in order to make good use of the whole range? In the example use a shunt resistor of 2mOhms but the current to measure is 10A, so the Vin+ - Vin- = 20mV
I think that I've to use a resistor of R=(Vin+ -Vin-)max/Imax=80mV/250mA= 320mOhm. Is it right?
Thank you so much, best regards.