Other Parts Discussed in Thread: INA219
Hi All,
I'm using an INA219 as part of a project to monitor the voltage/current on a 12v 110Ah battery. The INA219 is part of a breakout board by Adafruit:
http://www.adafruit.com/products/904
I've removed the 100R resistor there and using an external 50A 75mV shunt.
All was going well until suddenly it has stopped worked. I had switched the system off, then half an hour later switched it back on again, but looks like somehow may have damaged something. Vcc is 5V yet for some reason I'm now seeing a PD of 1V when measured between Vcc and GND with the INA219 board attached (removing it and the PD is 5V, so I know the rest of the system is fine).
I see reference to the INA219 having some kind of ESD protection that can be triggered by high dV/dt. I'm wondering if I might have triggered that somehow. Can anyone elaborate on what the protection is? Does triggering it damage the chip? Can is be reset?
Thanks
-Matt