Other Parts Discussed in Thread: LMP7721
Dear Sir,
Referring to the blog of Bruce Trump I have implement the current source design as mentioned in it. My current range is from 1pA to 1nA.
In this design I used the glass sealed 10G ohm of resistor with 1% tolerance and SD210DE MOFET with LMP7721 op amp.
The graph shows current with respect to voltage but it seems to have a noise of 10pA to it. And the Vs is maintained at 10 V. Vref is changed from 0 to 1.5V. This circuit is of current sink. And now I want to implement the circuit of current source, so instead of N-MOSFET I will have to use P-MOSFET. But while selecting P-MOSFET which parameters, I will have to consider. And in the above circuit where I am wrong let me know.