Other Parts Discussed in Thread: LMH6601, LMH6559, BUF602
HI~
I need to design an input 1.2V/1.8V/3.3V, the Buffer 400MHz of bandwidth. Please provide the recommended parts and circuits.
Thanks for your support!!
Eric
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Eric,
If you are looking for an amplifier to operate at a gain of +1V/V, you have some choices (but none that operate down to 1.2V supply voltage?):
LMH6601 (Op Amp, 250MHz, Vs_min= 2.4V)
LMH6559 (buffer, 1.7GHz, Vs_min= 3V)
The upper end of your supply voltage (3.3V, assuming you mean supply voltage) is not an issue and is covered with the devices I have listed above.
Regards,
Hooman
Eric,
Here is another choice:
BUF602 (Buffer, 1GHz, Vs_min= 2.8V)
Regards,
Hooman