Other Parts Discussed in Thread: LMC660, LMC6482, LMC6442, LMP7702, LMC6484, LMC6001, INA326, TINA-TI
Hi,
I have some lmc660 ic and I want to design a non contact active electrode my question is it suitable ic for replacing with lmc6442 or lmc6482 because I have 100 lmc660. Is it necessary for me to use exact lmc6442.
and the other question. I use the techneque that mentioned in lmp7702 data sheet for my lmc660 in simulate with TINA "
This input voltage noise can be
further reduced by placing N amplifiers in parallel as shown
in Figure 7. The total voltage noise on the output of this circuit
is divided by the square root of the number of amplifiers used
in this parallel combination. This is because each individual
amplifier acts as an independent noise source, and the average
noise of independent sources is the quadrature sum of
the independent sources divided by the number of sources" page 17
but not only it isn't good it is very bad and out put led to saturate.
Thank you in advance, and excuse me for any mistakes in the text as English that is not my native language
best regards,
Siyavash.