Other Parts Discussed in Thread: TL074, OPA134
Hello,
probably all schematics of operational amplifiers which I saw use for bipolar power supply two capacitors, let say 100n, each in one supply rail.
But for lot of years I use only one capacitor which is connected between +rail and -rail. (So no connecting to GND). The advantage is more simple PCB and VERY short path to OPA pins (only few mm), because I mount these capactors on bottom side of PCB directly next to power supply OA pins. Of course on board are other blocking capacitors as part of power supply. I solve here only local blocking of each OA.
So it works with TL074 and so on. But now I would like use more fast OA (OPA134 etc.).
So my question is if my solution is correct or which troubles may I expect .
Thank you in advance for your support.