Other Parts Discussed in Thread: OPA695, OPA684, OPA4872, THS3092, THS3091, THS3201, THS3202, OPA694, OPA691
Hi,
I'm a total newbie to choosing amplifiers and i need an operational amplifier to amplify a sine signal from 1Vpp to 10 Vpp (Gain=10) at a frequency of 50 MHz (maybe even upt to 200 MHz is this possible?), so which device would be the right one for me? or do i have to use multiple amplifying stages? And is is possible, in general, to get an op-amp with more than 1 in- / output?
Many thanks in regard