Other Parts Discussed in Thread: LMH6554, LMH6629, OPA653, OPA656, OPA657, THS4601, LMH6601, OPA2354, OPA2355, OPA2356, OPA2357, OPA3355, OPA354, OPA355, DEM-OPA-SO-1A, DEM-OPA-SOT-1A
Hi,
I have a voltage signal in the range of 10 µV which should be amplified by a factor of 104. The input impedance in the first amplifier is 100 kΩ. For measurement of the signal a digitizer card with input impedance of 10 MΩ is used.
Two LHM6554LE with evaluation board should be utilized for amplification:
- First LHM6554LE (differential input/differential output) with R2=R3=RG_P=RG_M=100 kΩ, RF_M=RF_P= 1 MΩ, R6=R7=2 kΩ, Gain = 10
- Second LHM6554LE (differential input/single ended output) with R2=R3=RG_P=RG_M=1 kΩ, RF_M=RF_P= 1 MΩ, R6=R7=3 MΩ, Gain = 103
Is it possible to run the amplifiers in this configuration? Thank you for your help.