Other Parts Discussed in Thread: XTR110
My XTR110 is set up for 0-5vdc in and 4-20mA out, and powered by 24vdc. I have been using the IRF9510 Pmos, but noticed its VGS is to low. The temperature of the IRF9510 at 20mA was 109.5F. I then tired the FQP2P20 Pmos and at 20mA its max temperature was 111F. I also tried the FQP7P06, which had a max temperature of 111F at 20mA. All the mosfets are capable of handling 2+ amps. Is this the reasion for the high temperatures at low currents?
What mosfet temperatures have other people seen?