Hi all,
I seen this website on the good answers and i would like to ask some question.I am building a 3 bit flash adc circuit using a reference of 8v with a string of resistor at 1k ohm each. I am using a Lm2903 comparator and although it is dual output and 4 inputs, i am only using 1 output and 2 input for each of the resistor. As we can see in between first and second resistor we should be feeding in 7v to the 1st comparator from the top and 1v to the last comparator.
It look something like this,
The input is lets say 3.5 volt,
at the 4rd comparator from the output is near 0v due to 4v bigger than 3.5v but at the last 3rd comparator when input is larger than 3v, it outputs a 1.3v.The result of output 1.3v is same when compared at last 2nd comparator. I am feeding the VCC of the comparator a voltage of 18Volts. However at the last comparator, when 3.5v is larger than 1v, it now gives only a 0.4v. Why is that so? also Why is the output 1.3v and not 5v for logic '1'.
btw I am new on this. Sorry for any trouble