Other Parts Discussed in Thread: VFC320
Dear Bruce Trump,
We are using VFC 320 in our application for the range of 0 to 10 V input output of 0 to 100 KHz.
The circuit was calibrated in the room temperature (24°C) and tested for more than one week in the lab.
When the circuit was deployed in the field (Approximately 30 to 40°C), the output started to reduce. Up on investigating, it was found that the output is varying drastically depending on the temperature. It was also noticed that the output is back to normal when tested at room temperature again. The drift was around 100 to 150 Hz
The supporting components used are all high precision and all the components are tested individually for the temperature dependency. During the individual test, it was found that VFC320 is contributing to the drift.
Please let me know how to tackle the issue.
Expecting your reply,
Regards,
Madhu.