I am trying to use XTR117 in an application to control the current like a 4-20mA transmitter.
The trick is that the external sensing circuitry is not on the IO pin, it is on the V+ pin.
So in this case, there is the 24VDC loop power supply, the sensing circuit (250 ohm resistor), then the XTR117, and the IO pin goes back to the loop power supply (-).
I have multiple XTR117's connected to a single octal DAC. I am not connecting anything to the VREG pins of the 8 XTR117 parts.
What should I do with IRET?
I want all the of the current that comes in on the V+ pin to go out the IO pin, because in my circuit, the measuring device is on the V+ side of the part, not the IO pin side.
I think IRET has to be grounded so that it is the same potential as the DAC reference ground.
But will having mulitple XTR117's connected to the same ground allows for currents to flow in or out of the IRET pin causing problems for my controlled current coming into V+?
It looks like the part really wants to control the current coming out of the IO pin. that will work for me if I can make sure that all the current going into V+ comes out the IO pin.
In my current design, all 8 IRETs are connected together along with the GND from the octal DAC.
Is that a problem?