Hello,
I have to send an analog voltage signal over an optical link. I would like to do this by a V-F -> F-V conversion.
The problem is that the voltage hase some short spikes (1ms) which have to be recovered on the "other side" by the F-V conversion. This image shows the input signal which has to be transmitted:
Its not important to recover the exact height or width of the spikes, but they must be visible.
Can I do this with the VFC32 / LM231? Is the speed / resolution good enough?
Many Thanks for any answer!
Best Regards,
Stefan Baehring