Other Parts Discussed in Thread: TLV3402, TLV3401
Dynamics Inc. is having an issue with the TLV3402 output going high and then never changing states again even when the input should cause it to go low. They are unwilling to give a schematic but they did give me a description of what was happening. Their comments are in blue:
"I’m wondering this because we’ve been seeing a situation where it appears that when the comparator turns on and the output goes high, then it never changes state even though the inputs to it should cause the output to be low. It’s a very rare situation, but I happen to have a couple of scopes hooked up and monitoring different points on the comparator as well as other points on the card when I saw it happen. Is there some case that could cause this chip to latch up?"
I asked him for a description of how the device is being used:
"Basically I have the comparator voltage at 2.7V and I have the output voltage pulled up to roughly 3.5V. Its connected to 4.1V through a diode and a 100k in series. Can you double check if there are protection diodes on the output and that we can only go to approximately 0.5V above Vcc? I thought one of the benefits of an open drain output on a comparator was that you could use a different voltage there instead of needing to level shift? Also, the comparator doesn’t normally stay on so we’re constantly turning it off and on. Normally it appears to work without a problem, but once in a while when we’re turning it on and off faster than normal it looks as though the output goes high on start-up and stays high with the inputs set so that the output should be low."
I talked with Thomas Kuehl about the protection diodes, and we decided that they wouldn't be causing an issue like this. Gave that feedback to the customer and got this reply:
"It looks like the latching up may have something to do with timing. When I watch the two inputs and the Vcc of the chip rise it appears that they rise from 0V to their respective voltages in about the same time. Vcc is rising to 2.7V in about the same time that the plus and minus inputs rise to their voltages, which are about 2V and 1.5V. The latch-up problem seems to become less frequent if I ground the output of the comparator for approx. a 1ms. Since this seemed to improve things I also decided to ground (the input is not actually at ground, but maybe it’s held to approx. 0.5V) one of the inputs to the comparator as well as the output. If I ground the output and the an input for approximately 500us when powering up the chip it appears to get rid of the latch up problem. Is there a spec. for how long I would need to wait to apply voltages to the inputs after power for the chip has come up? Again, this doesn’t happen every time, just every so often."
I was hoping you could help me answer the last question specifically and any additional assistance in determining the cause of this problem would be great as well. Thanks!