Hi,
We have a device in production which has a single stage Transimpedance Amplifier OPA657 in Die form. (Feed back resistor Rf = 10k ohm)
The question is:
If I connect the output of the device to a
1) Oscilloscope: The power supply draws +/-10mA of current irrespective of the Load (50 ohm or 1M)
2) Spectrum Analyzer GSP810: Same observation as DSO
3) DSA 3561A: The power supply draws +40mA/-10mA of current as soon as I connect my device to the Input.
Also, if I change Rf from 10k to 50k, the DSA 3561A draws +/-10mA. We dont understand why?
Any suggestions will help. We use DSA3561A to measure Noise density for our device.
We have to deliver this assignment y next week and hence, it is very critical.
Thanks,
Ankur