Other Parts Discussed in Thread: XTR111
Hello,
can you please help on below questions (bottom of mail) from my industrial end customer FESTO.
Thanks a lot in advance !
Regards
Günter Fettig
Reference: Datasheet XTR111, Figure 3a
Using the XTR111 as current output (4-20mA) for a new circuit, I am struggling to design the external current limit perfectly. Only the circuit 3a (gate controlled current limit) is possible in this application because there is no possibility to implement a heat sink for a second large transistor as it would be necessary for the serial current limit 3b.
Thanks to a discussion on the Ti Website Link, I think that I understand the principle of this current limit correctly. With currents well above 20mA, the voltage drop at R6 should reach the Base-Emitter (turn)-on voltage of Q2. This will clamp the gate of Q1 to its source, and so limiting the possible current flow through Q1 (to the load).
I want to use a BC807-40 PNP transistor for Q2. The circuit should be working correctly from -25°C up to (at least) +100°C. With higher temperatures, Q2 will turn-on much earlier and so limiting Iout to lower values. With the datasheet-information (figure 38 and chapter “EXTERNAL MOSFET” ) I made some simulations of the current limit and found out, that R6=18R would be a good choice.
Parameters:
Temperature -25°C ... +125°C (50°C steps)
VSP = ~IS = 30V
VG = VSP-16V = 14V
Internal resistance of VG-Drive = 3k
Q1 = BSS84 (for simulation only, design will be with a BSS192, no simulation model for this)
Simulation:
Results:
I_RLoad is limited to max. 40mA (-25°C) and min. 24mA (+125°C)
I_VSP (the current that should be limited to 50mA to protect the XTR111) is restricted to max. 44mA (-25°C) and min. 28mA (+125°C)
Using and testing exactly this circuit in the lab, I can see that the I_RLoad current of 20mA is starting to decrease with higher temperatures starting from +60°C. The reason (with a very high certainty) is the external current limit: If I remove Q2, everything works fine up to +120°C, with a nearly stable current at the output. I already tested to use R6=15R with no real difference in the behaviour.
Additional information: At high temperatures (+110°C), Vin is stable and R_Set is stable, R6 is stable.
Question 1: Is there anything fundamentally wrong with my simulation model, or with my understanding of the circuit?
Question 2: What resistor would be recommended by the experts using a BC807-40? Is the BC807-40 a completely wrong choice?
Question 3: What else could be the reason for this behaviour?