First question:
I'm developing device, which uses LOG114 log amp. I'm hobbyst, so I need to solder this chip "by hands" with hot air resoldering station, without soldering mask and "professional" equipment (my home technology allows me to make accurate enough board for this package, but it is pure copper, without mask).
Should/must I connect thermal pad to V-? Datasheet says "Yes", but user guide of evaluation board contains top copper drawing and it doesn't look like here are connection between thermal pad and V-.
Second question:
Now I have "breakout" board, which converts QFN16 to DIP16-like package, and I have strange behavior of LOG114 on it: there are NO connections between any two pads/pins, but LOG114 doesn't work properly on it. Ref source gives stable 2.5V, but LOG out is near V+ or V- without any in-between values no matter which currents are connected to I1 and I2 (via resistors from VREF).
I use+/-5V bipolar supply from galvanic batteries now, for experiments.