This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Temperature extremes in LMV841

Other Parts Discussed in Thread: LMV841

Hi!

In the data sheet for the LMV841, it states that the boldface limits applies to temperature extremes.

Can the assumption be made that this applies in fact to the temperature range 85-125C, or what is temperature extremes?

Please help me to clarify this!

Thanks for the support,

Martin Gustafsson

  • Hello Martin,

    "Extremes" mean both ends of the temperature scale. Bold indicates across the entire specified temperature range, listed in the "Operating Ratings" section, which would be -40°C to 125°C.

    So that means the device should be within that spec between -40°C and 125°C, which would also include 85°C.

    Regards,