Which is Vcc(Max) of LM2902KPWR ,26V or 32V?
The 5-page of the datasheet is set to 26V, and others have become 32V only LM2902.
The 3-page of the datasheet is 26V.
Which is right?
Thank you for your consideration.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Which is Vcc(Max) of LM2902KPWR ,26V or 32V?
The 5-page of the datasheet is set to 26V, and others have become 32V only LM2902.
The 3-page of the datasheet is 26V.
Which is right?
Thank you for your consideration.
Satoshi,
The maximum is 26V for the LM2902KPWR.
LM2902KVQPWR is rated and tested to 32V.