Other Parts Discussed in Thread: OPT101
Hi, I want to measure little amount of light power with the opt101. I tried the basic circuit like in datasheet with 9V on pin 1, ground connected on pins 3 and 8, 0.1uF decoupling capacitor on pin 1 and I shorted pins 4 and 5 together. It works, but instead of getting around 7.5mV of dark current, I get around 70mV when I measure in absence of light. I tried 0.01uF capacitor instead but same result. Also, I tried another chip but same result.
I don't mind having a 70mV offset but I just want to know if its normal and if I'm gonna get the right signal out of it.
Thank you