This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMP91000 circuit design?

Other Parts Discussed in Thread: LMP91000

Hello!

I am working on an oxygen sensor which is alphasense O2-A2. I designed a circuit with lmp91000,but i could not solve sensor reaction time. I mean that, when i start my system,sensor does not start in 6 - 7 minutes. It is always show maximum oxygen concentration, then it is starting decrease slowly to real concentration. But it is showing right concentration after 1 hour!.....

Here is my register configurations;

TIA_Gain = 14K

RLoad = 10R

Ref_Source = internal (Vdd = 5V)

INT_z = 67%

Bias_Gain = positive

Bias = 0%

Fet_Short = Disabled

OP_Mode = 3-lead amperometric cell

On my circuit design;

between C1 and C2 10 pF and 1 Mohm paralel

all grounds connected together

I have tested my i2c communication about writing to lmp91000, and there is no problem.