Can OPA2188 be used as a comparator?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Daniel,
The OPA2188 has diode clamps across the input terminals. See this link for a discussion of how this can affect use as a comparator...
Op Amps used as Comparators—is it okay?
These clamps will behave as a diodes with a series resistance of approximately 1k-ohm. If you limit the differential input voltage to a few hundred millivolts, it could be used as a comparator and you probably would not notice the clamps. If you have enough differential voltage to really turn on the clamp diodes, expect that pretty high currents could flow. I suggest that the differential input voltage should be limited to 5V or less at which point you would have several milliamps of input bias current.
Regards, Bruce.