HI,
I have a design were I am using the OPA551 as an integrator. Positive supply is at 60V and the negative is at 0V.
The inputs are at +2.5V from the negative supply, which is at the low end of the permitted input range.
My concerns are:
1. Does this low input common mode level degrade input noise levels?
2. Can de device sustain low noise levels over temperatures?
BR
bjarke