This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

To reduce noise in INA105 difference amplifier circuit

we are using INA 105 in one of our instrumentaion applications.  The range of signal we intend to use is from 0mV to 30 mV. We are using in differential mode with Unity gain.  The problem we are facing is the noise obtained is around 150mV. We have used sufficient bypass capacitors across +/-15vdc supplies.  Kindly provide a suitable method to limit the noise to near zero mV.