Hi, my name is Daeyoun Yun.
I have any questions(PGA309EVM-USB and Multi-Cal-PGA309).
First, look at the PGA309EVM-USB evaluation module, I know to make a calibration using the PGA-test board.
If, without using thd test board, what should I do wiring connection when using the real-world pressure sensor(PGA309 built-in)?
Second, always needs RS232 communication of the DMM when the calibration by using the Multi-Cal-PGA309 (I used the Multi-Cal-System = sofrtware)?
Do not have to be calibrated via a wire connection without using an RS232 communication?
Finally the DMM script that is attached to the software, do I want to be a used to modified?
When used without changing the DMM script, the calibration is not performed.
For example,it was confirmedthat the outputvalueof theactualchange, butVoutshown inPC monitordid not change.
I look forward to your reply.
Thank you.