Other Parts Discussed in Thread: TPL0102-100, OPA378, OPA330, OPA335, OPA376, OPA188, OPA333, OPA2180
I am using an OPA378 as a buffer on a reference. It is configured as a unity gain buffer, with an RC filter (1MEG series, 15nF shunt) before the noninverting input, and followed by a connection to pins 3 and 4 (high terminals) of a TPL0102-100 (digital pot). The low terminals are tied to ground so this looks like a 50K load.
V+ of the OPA378 is just shy of 3.3V. V- is at ground (measured). The input to the RC filter should be 500mV but in circuit is 478mV. The NI input of the OPA378 is at 436mV so there is a 42mV drop across the 1MEG resistor (well beyond what the bias current would normally cause). The output of the OPA378 is at 497.6mV even though the output is tied to the inverting input...no gain resistors.
I have looked with a scope and all of the waveforms are solid DC...no oscillations.
If I remove the input RC filter and inject a DC signal from a reference directly into the NI input, the amplifier works perfectly. I have used RC filters on the NI input of opamps before without a problem. The application required a very low-noise reference so I would prefer not to remove the RC filters. I'm well within the CM spec for the part.
Any idea as to what is causing the problem?
Tim