What isthe input impedance of OPA360 and also LMH730216 ?
Regards,
-Jaden
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Jaden,
LMH730216 is an EV Module PN. What is the OA Part No.?
Jaden,
TINA-TI had a model for the OPA360, so I ran an AC Analysis transfer function for Iin/ Vin (see attached screenshot) then inverted to get Vin/Iin = Zin. At 10 Hz, Zin is around 562 M ohm and at 10 MHz, Zin is around 1k ohms. I think this looks about right but is model dependent.
The LMH 6704 does not have a TINA-TI model but the input is specified to be 1 M ohm in parallel with 1 pF typical so this covers the gain of +1 and +2 cases. For the gain of -1 case, the input impedance is just the input resistor value of 465 ohms (likely with 1 pF cap to GND).