Other Parts Discussed in Thread: THS4121, THS4521
Hi!, I have a few questions about fully differential amplifiers. Im doing an EEG, for my thesis to become an electronic engineer. And I was wondering if it is possible with this amps ( or any configuration with 2 or more of this kind of amps) to make a very high CMRR circuit. At the amp output, the signal mantaines differential, but ones stage CMRR's, acts in chain with the other stage CMRR's increasing it? For example:
Stage 1: Buffer (voltage follower with Gain=1), CMRR 60dB, fully differential (diff input, differential output)
Stage 2: Insturmentation amplifier, differential input, single-end output, CMRR 80dB, Gain=500
Entire Circuit: Gain=500, CMRR=60dB + 80dB = 140dB, single-ended output
Is this possible? Can i increase the CMRR with more than one fully diff amp like THS4121?
My contact email is leoyanzon@hotmail.com
Thanks!