This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMV358 Upgrade

Expert 1485 points

Other Parts Discussed in Thread: LMV358, TLV342A, OPA2376

I am looking for a new dual OpAmp to provide better performance than the LMV358 that we have been using.  Here are the requirements:

  • Industrial temp range
  • Standard SO-8 package / pinout to match LMV358
  • Gain Bandwidth product > 1MHz
  • Power supply range 3.0 to 5.5V
  • Rail-to-Rail input and output (within 100mV at 2k load)
  • Input Offset < 51uV

In general, it needs to be low power, low noise and low drift, but I do not have hard specs on these as they are tradeoffs.  The price target is $0.50 per dual amplifier in volume (50k per year).