Other Parts Discussed in Thread: THS3091EVM, THS3091, TPS2024
Hi,
When I debug THS3091 according to following configration(Power supply is +_15V,G=5,and the input is +_2V bipolar signal),when the input signal's frequency is 1MHz,the output is right(+_10V,20Vp-p),but when I increase the frequency of input signal,THS3091's output amplitude will decrease,as per my test, the output(Voutp-p) with 2MHz input signal will start to decrease,but it's normal and right for below 2MHz input signal. After I check,when the output decreases,the input signal's amplitude decreases(Vinp-p) too.In THS3091's datasheet,the BW is about 190MHz with G=5,should be enough,and its SR is enough high too. I also tested on THS3091EVM,the phenomena was same.I don't understand why this input signal decreases along with input signal's frequency increase,because of THS3091's Noninverting input capacitance? Would anybody like to help me?Thanks in advance.
Best Rearge
Li