This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Need some help determining reference value for bridge amplification circuit.

Other Parts Discussed in Thread: INA122

I am using the INA122 to amplify a mV signal from a strain gauge.  My basic circuit works, but it appears that I am falling below the 100 mV minimum input which is causing linearity errors.  This is my spec's.

 

Vcc = 2.5V single supply

Gain R = 425 ohm

The strain gauge is a 350 ohm 2 mV/V output(0 - 5mV).  My a/d has a range of agnd to 2.5V.  I am probably going to have to bias this as well.

 

So what I am looking for is how to calculate the appropriate ref voltage to give me a 150mV to 2.3V output.

 

Thanks in advance.

  • Kevin,

     

    I would recommend reducing the gain and then placing a voltage on the Ref terminal to offset the output signal. Maybe a 500mV reference? The datasheet mentions that the voltage applied to the Ref terminal is added to the output signal. Refer to Figure 2 (page 7) of the datasheet for a circuit to help trim the offset voltage. Hope this helps!

     

    Sincerely,

    Alex