Other Parts Discussed in Thread: OPA695, OPA847, TINA-TI
I plan to use a photodiode in a room (with 120 Hz background light) to pick up very weak laser pulses (pulse width 50 nS). Can I use only one stage current feedback amplifier (e.g. OPA695, single 5V)? Is it easy to filter out noise < 5 kHz? The photodiode: rise time = 6 nS (for Rload <1000 ohm), capacitance = 5 - 6 pF, dark current = 10 nA. Thanks.