Other Parts Discussed in Thread: ISO124
Hello,
This is a question on TI part ISO124, which is an Isolation Amplifier.
I never used it before, but the data sheet states that the power supply voltage is +/-4.5V Min and +/-18V Max.
1. Do I need both plus and minus power supply (+Vs1 and -Vs1), if my input signal is +1.5V and changes with time to 0.2V Min? May I ground -Vs1?
2. Do I need +Vs2 and -Vs2, if I am expecting +1.5V at the output, or I can put -Vs2 to GND? (Gain is 1 in accordance with data sheet).
3. May I use different voltages, e.g. Vs1=+5V, Vs2=-15V?
Thanks in advance for your help,
Alex.