Hello,
I need to bias an on-chip coil of ~1uH (R~10Ohm) with rectangular current pulses of 2A, duration 1usec, rise time < 50nsec. I can do it with AWG Agilent 33250A (80MHz), but only to the level of ~200mA. I need either to amplify the signal from Agilent or get a separate AWG of high, fast output current. Could you recommend me an amplifier or AWG that would solve my problem? Thanks.
Maciek