Other Parts Discussed in Thread: THS3091, OPA691, OPA690, OPA2674, OPA2673
hello i want high speed high current op amp for 10MHZ function generator which i developing and can match to 50R output thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
We have a lot of device that can match your needs.
For ±15V operation, look at the THS3091.
For ±5V operation, look at the OPA2673, OPA2674, OPA690 or OPA691 for a single amplifier.
You can also increase the output current drive of most amplifiers by paralleling them together. The following app note will also point you towards additional high speed, high output current line drivers. http://www.ti.com/lit/an/sboa127/sboa127.pdf