Other Parts Discussed in Thread: LMV611, OPA544, LM675, LM386
Hi
I am trying to use lmv611 in order to generate wave generator.
I am building simple wein bridge (see below) where: r1=r2=160k, c1=c2=100n rf=20k rb=10k (f=~10hz).
1. without a load I get to cut sin wave - the max amplitude is cut at 4V because when I set my power source to -5-5 the current raise and the amplifier stops working - it is strange for me because it suppose to work until 5V . so how come the amplifier cant work in -5-5V?
2. when I connect the load same phenomena happens juts now it is cut at 0.6V. Is it because the currents are to high (150mA)?
R-load=~8ohm
Does the reason is the high currents?
which amp is better for me in order to achieve 250mA currents on that load?
thanks in advanced,